Feedback_Iq_Min
Feedback_Iq_Min
| Address: | 10259 (2813H) |
| Type: | UINT16 |
| Access: | Read/Write |
| Unit: | mA |
| Range: | UINT16 |
| Default Value: | 500 |
| Store Supported: | Yes |
| Description: | This value is used for Feedback feature and define the minimum amplitude of the phase’s current. Can be considered also as minimum current applied at the motor |
| Notes: |
See Closed Loop Modality for details. |